2020-03-29 10:43 AM
I use CubeIDE 1.3.0 and STM32L4 MCU Package 1.15.1.
I wanted to setup a demo project for Nucleo-L4R5ZI.
these boards route LPUART1 to STLINK debug Uart port.
If you enable NVIC for LPUART1, the firmware package creates a faulty IRQ handler. It should pass HLPUART1 to the IRQ handler but it passes HUART1 (which is not used and not initialized)
void LPUART1_IRQHandler(void)
{
/* USER CODE BEGIN LPUART1_IRQn 0 */
/* USER CODE END LPUART1_IRQn 0 */
HAL_UART_IRQHandler(&huart1);
/* USER CODE BEGIN LPUART1_IRQn 1 */
/* USER CODE END LPUART1_IRQn 1 */
}Workaround:
void LPUART1_IRQHandler(void)
{
/* USER CODE BEGIN LPUART1_IRQn 0 */
HAL_UART_IRQHandler(&lphuart1);
return;
/* USER CODE END LPUART1_IRQn 0 */
HAL_UART_IRQHandler(&huart1);
/* USER CODE BEGIN LPUART1_IRQn 1 */
/* USER CODE END LPUART1_IRQn 1 */
}
Solved! Go to Solution.
2021-03-02 9:23 AM
Hello @jvisser,
Good news :) I am pleased to inform you that this issue is fixed in the latest STM32CubeMX version 6.2.0.
The LPUART1 IRQ Handler is correctly generated by CubeMX.
Thank you for your contribution.
Khouloud.
2020-04-17 10:01 AM
Hi @Johannes ,
Thanks for bringing this issue to our attention. It is reported to our STM32CubeMX development team.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-03-02 9:23 AM
Hello @jvisser,
Good news :) I am pleased to inform you that this issue is fixed in the latest STM32CubeMX version 6.2.0.
The LPUART1 IRQ Handler is correctly generated by CubeMX.
Thank you for your contribution.
Khouloud.