2025-10-14 7:13 AM - last edited on 2025-10-14 7:28 AM by Andrew Neil
As of yesterday, since an update hit, my CubeMX view won't render (literally it is just a white background). Tried reinstalling and it renders, until I sign up and it updates again, then it stops rendering again. The rest of the IDE works just fine.
System:
Ubuntu 24.04.3 LTS (Linux 6.14.0-33-generic)
Dell Inspiron computer
8,0 GiB Memory
Wayland windows system
Gnome 46
CubeIDE 1.19.0
2025-10-14 7:31 AM
Hello @bussy_user
Let's try using a Fresh Workspace by following those steps :
- Start STM32CubeIDE.
- When prompted, select a new, empty workspace directory.
- Import your existing projects into the new workspace
If the Issue Persists: Clear the .metadata Folder
- Close STM32CubeIDE.
- Navigate to your current workspace directory.
- Delete the .metadata folder
- Restart STM32CubeIDE.
- Re-import your projects into the workspace.
I will be waiting for your feedback.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-14 8:10 AM - edited 2025-10-14 8:16 AM
Done in order:
It didn't work. Even with new projects it doesn't work.
2025-10-14 8:36 AM
Hello @bussy_user
As a workaround, please try using the standalone STM32CubeMX , you can download it from the following LINK
I am currently investigating this behavior internally and will update you as soon as I have more information.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-10-14 10:03 AM
Same over there:
-I downloaded it
-Configured the chip -> "code generation requires packages, please log in"
-log in -> downloads updates and or packages
-tried to generate code -> app doesn't work anymore (freezed)
-close it -> open it -> tried to open the .ioc -> it doesn't open anymore