cancel
Showing results for 
Search instead for 
Did you mean: 

Component: Simulink| Category: Block diagram error Refer to the filed that does not exist 'codeFormat'.

LXion
Associate

The matlab version is 2019a;

The STM32CubeMX version is V520;

The stm32-mat/target version is V442;

I use matlab&simulink and stm32CubeMX to develop stm32f746Discovery.

For more information, please refer to the attachment

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Brian McKay
Associate III

I don't know if the STM32-Mat/Target has been tested with R2019a, nor do I know if this is the issue.

You may want to try R2018b or R2018a.

Cheers,

-Brian

Kg
Associate

I have a same error, did you have solve it?

Cyril FENARD
ST Employee

​Hi,

This problem is solved with the version 5.1.0 of STM32-MAT/TARGET, published end of July 2019.

Regards.

Cyril