cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot find stm32l4xx_ll_gpio.h after cubemx generate code

charlie239955_st
Associate
Posted on August 22, 2016 at 01:30

I had built a project with cubeMX and I had been working on it.

I wanted to make a change in the configuration, so I ran CubeMX and re-generated the code.

Only this time, CubeMX did not include the  Drivers/Inc/stm32l4xx_ll_gpio.h file in the project.

I need that .h file because I use GPIO_PIN_RESET and GPIO_PIN_SET macros, and I use LL_GPIO_ReadInputPort.

Why would cubeMX stop copying the stm32l4xx_ll_gpio.h file to the project?

#stm32cubemx-stm32l4xx_ll_gpio.h
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Walid FTITI_O
Senior II
Posted on August 22, 2016 at 11:23

Hi hand.charles,

I submit your request to our CubeMx team to investigate why the current version of CubeMx doesn't integrate the ll_peipheral.h files the project workspace automatically.

-Hannibal-