cancel
Showing results for 
Search instead for 
Did you mean: 

Bug Report: CubeMX Generates Bad Init Code

Sidlauskas.David
Associate II
Posted on March 17, 2018 at 21:08

Using CubeMX V4.7.25.0 I get initialization code for RTC.c that won't compile when I request initialization be generated as .c.h file pairs.

Simple demo case:

Start CubeMX

New Project

Select STMf103C8Tx as target

Under Pins Select RTC-> Activate Clock Source.

Under Project settings:

   Project Name: Test

   Location: C:\Temp\

   Under Code Generator Tab:

         Check Generate peripheral initialization as pair of .c/.h files

Generate code for TrueStudio

When I build the generated code I get the following errors:

..\..\..\Src\rtc.c:73:5: warning: implicit declaration of function 'LL_PWR_EnableBkUpAccess' [-Wimplicit-function-declaration] LL_PWR_EnableBkUpAccess();..\..\..\Src\rtc.c:75:5: warning: implicit declaration of function 'LL_APB1_GRP1_EnableClock' [-Wimplicit-function-declaration]  LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_BKP);..\..\..\Src\rtc.c:75:30: error: 'LL_APB1_GRP1_PERIPH_BKP' undeclared (first use in this function)

     LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_BKP);

                            

If I generate code for the test project with the peripheral inits in main(), the project will then build without error.

Is this a CubeMx bug?

Dave

#cubemx-bug-init.-code
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
imi415
Associate II
Posted on March 18, 2018 at 15:48

As a temporary workaround, I replaced these lines with which generated by older version of CubeMX.

However, this will be replaced back by CubeMX after re-generation.

LL_PWR_EnableBkUpAccess

();

/* Enable BKP CLK enable for backup registers */

LL_APB1_GRP1_EnableClock

(LL_APB1_GRP1_PERIPH_BKP);

Replaced with:

HAL_PWR_EnableBkUpAccess

();

/* Enable BKP CLK enable for backup registers */

__HAL_RCC_BKP_CLK_ENABLE

();

Imen.D
ST Employee
Posted on March 22, 2018 at 15:25

Hello,

This is knownissue already reported to CubeMx team for fix.

https://community.st.com/0D50X00009XkWuZSAV

Sorry for the inconvenience it may bring.

Kind Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on June 05, 2018 at 16:00

 ,

 ,

I put this code into the user code section before the problem code to avoid the CubeMX code replacement:

♯ warning These definitions is a temporary workaround. Remove them, when the STM32CubeMX bug will be fixed.

 ,

♯ define LL_PWR_EnableBkUpAccess() HAL_PWR_EnableBkUpAccess()

 ,

♯ define LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_BKP) __HAL_RCC_BKP_CLK_ENABLE()