cancel
Showing results for 
Search instead for 
Did you mean: 

Board configurations in a single CubeMX / Truestudio project?

Mttjcksn
Associate III

Hi there,

I have been developing a CubeMX generated project in TrueStudio for the STM32H7 EVAL board.

I would like to get the same project running on the H7 Nucleo board, and then eventually on my own hardware.

I'd like to keep configurations for all three boards in a single project and select the configuration I want to compile for.

Is it possible to have multiple configurations in a single CubeMX project?

Is it possible to have multiple configurations like this in TrueStudio, and if so, what is the easiest / best way?

Many thanks!

Matt

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Mttjcksn
Associate III

CubeMX seems to put all of it's pin assignments in main.h. So I guess one solution would be to remove the pin allocations that are different between the two boards from the CubeMX project and put them into a 'user code' area in main.h with compiler flags to select assignments based on a selected build configuration.

Does that sound sensible?

Thanks,

Matt

Mttjcksn
Associate III

I tried removing the pin allocations from the CubeMX project (which was really tricky because they come in a peripheral 'block'), but unfortunately then the generated MSP files just then reference a specific default pin rather than a generic name, such as 'LED1_pin' that you can define a pin to yourself.

Surely someone has managed build configurations for different boards here... anyone?