2020-02-02 11:08 PM
Hi,
if i record the power everything looks good like:
but, if i zoom in/out or press "Show All" it looks like this:
Anyone else using this feature?
Solved! Go to Solution.
2020-03-18 04:32 AM
Dear aritec,
New release 1.1.1 is available on st.com. Can you download and test if it's solving your issue ?
Thank you
2020-02-28 02:59 AM
Hi aritec,
Data are subsampled to be displayed in the chart ( reducing the amount of points to avoid crashing the graph ). In your case it seems that the subsampling ratio is very high ( keeping only min and max values ).
Can you share the Data log ?
Thank you
Landry
2020-03-01 10:15 PM
2020-03-02 12:37 AM
Hi Aritec,
A Data Log is composed of at least 3 files :
There is an issue with your data log as the rawlog file is not available in it : 2020_03_02_07_07_27_1_rawfile_1.csv .
I don't know yet why , but can you check on your side that when you perform an acquisition something is stored under :
"YourUserDirectory"\AppData\Local\Temp\Power_Monitor\Acquisition\
You should find here one directory for each acquisition with inside at least the 3 files mentioned.
Thank you
Landry
2020-03-02 12:48 AM
Aritec,
The path mentioned was for windows , for mac, acquisitions are stored under :
"YourUserDirectory"\Library\Power_Monitor\Acquisition\
Landry
2020-03-02 01:14 AM
Aritec,
I reproduced the issue on our side. Let me come back to you asap
2020-03-02 08:50 AM
I confirm the issue and solution found. I will deploy a new release (1.1.1 ) asap
2020-03-02 08:52 AM
Thank you Landry
I'm looking forward for it.
2020-03-04 09:10 AM
Hi aritec,
Official release will be available in 2 weeks from now.
Best regards,
Landry
2020-03-04 10:18 AM
:thumbs_up: Thanks, I'll test and use it.