cancel
Showing results for 
Search instead for 
Did you mean: 

Conditional Data Logging

VOlet.1
Associate II

I want to in corporate conditional data logging in Cube Monitor Flow, since i intend to monitor the behaviour over many hours.

My requirement is to log all the 4 fields:

ms_enDeviceOrientation

ms_stStAccelDataX

ms_stStAccelDataY

ms_stStAccelDataZ

only if ms_enDeviceOrientation changes from value of 1 to value of 2.

I tried to tie this to the trigger threshold in data acquisition but this option was disabled.

Could not find any examples to do this any other way.

Looking forward to clear and specific description or example.

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11

Hi @VOlet.1​ ,

For the x , yes it's a running counter in millisecond, no you can't set it by your own but when you load data in the graph by default the first point is set to 0 .

For the content of the log file, you are right it's not readable with a basic json parser. We should correct it.

Landry

No update since a while, closing the post.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.