2024-11-15 08:27 AM
Please look at the screen shot:
I presume that the NUCLEO-H7S3L8 is equipped with a STM32H7S3L8H MCU... This is also what I can read on the MCU.
Thank you.
Solved! Go to Solution.
2024-11-15 09:47 AM - edited 2024-11-18 01:43 AM
Hello @tcachat
You are right, this board is equipped with the MCU mentioned under the column mounted device. It should be a typo in the description. I've escalated internally for correction on the future (under internal ticket number 196460).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-15 09:47 AM - edited 2024-11-18 01:43 AM
Hello @tcachat
You are right, this board is equipped with the MCU mentioned under the column mounted device. It should be a typo in the description. I've escalated internally for correction on the future (under internal ticket number 196460).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.