cancel
Showing results for 
Search instead for 
Did you mean: 

What is wrong with STM32 CubeIDE IOC editor?

PanutaRoman
Associate II

Hello,

For some time the CubeIDE ioc editor looks like this:

PanutaRoman_0-1728930582741.png

How can I fix it?

BR, Roman!

1 ACCEPTED SOLUTION

Accepted Solutions

Could you try to unistall and re-instal the last version of the STM32CubeIDE. It may solve the issue.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
STTwo-32
ST Employee

Hello @PanutaRoman and welcome to the ST Community :smiling_face_with_smiling_eyes:.

Have you updated your STM32CubeIDE to the last version (V1.16.1). 

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello @STTwo-32 

Yes, I have latest version (v1.16.1).

BR, Roman!

Could you try to unistall and re-instal the last version of the STM32CubeIDE. It may solve the issue.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello,

It solved the issue. But why this happen and really need to reinstall tool to fix some GUI issue?

BR, Roman!

enoughstatic
Associate

Not sure if the issue I am experiencing on Mac STM32cubeIDE is similar, but without updating, just out of nowhere(?), the .ioc file looks terrible.

Contrast is too bright.

Headers within some panes are missing, such as interrupts--which means how do you know what the checkbox is doing for a given interrupt?

When trying to add a User Label, such as for the GPIOs, once you start typing, the character you entered is highlighted. Once you type the second letter of your intended user label, the next entry overwrites the character. Instead, you must use the right-arrow key (on your keyboard) to move to the next character.

Very painful and annoying bugs that I have a hard time believing much testing, if at all--was conducted.