cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE "Error Downloading the following files: crdb_full.zip (Cannot unzipped)"

Ec1
Associate II

Hello.
I encounter this problem when creating a project with STM32CubeIDE. How can I solve it.

Ec1_0-1711740366732.png

 

 

 

 

7 REPLIES 7
Ec1
Associate II
 
JJORDAN16
Associate

Hi, I have also been having this problem. I installed version 1.15.1 and I tried to create a new stm32 project and I got this exact error.Were you ever able to resolve it? I saw the same issue in some other threads, but none of those solutions worked.

Thank you so much! Earlier, I had tried using my phone's mobile hot spot like you suggested and it did not work. But, I tried again today, and it worked!

I am glad that your problem is solved. You can subscribe to www.ertansuluagac.com and ask your personal questions in the contact section.

 

FluxPower42
Associate III

Hello!

I think you have fixed the problem by now. But maybe someone who has the same problem will be interested.

I had a similar problem when I tried to install the SMT32G474 package.
After I moved the folder for the firmware repository from my user directory to a general directory on the C disk, the problem no longer occurred.
You can find the settings under: [Help/Connection & Updates] and the [Updater Settings] tab in the dialog.
In the [Firmware Repository] section, I set the directory to
C:\Local\Tools\STMicroelectronics\STM32Cube\Repository
But all other generally accessible directories without spaces(?) should work.
It was then possible to install the packages.

With kind regards,
Timo

Windows now has symbolic links. So instead of moving stuff to C:\Local\Tools\STMicroelectronics\STM32Cube\Repository you can create a symlink to the "repository", that has a good name. Enter this name into CubeIDE or MX settings. Now you can access the "repository" by either name.

Well, Local\Tools\STMicroelectronics\STM32Cube would be real directories, and 'Repository' would be a symlink created in the latter directory.