cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to import USBD_Composite_STM32H503 froject from stm32-hotspot

Anirudhoruganti
Associate II

I have stm32cubeIDE version 1.17.0 and I'm not able to import this project and build it: https://github.com/stm32-hotspot/USBD_Composite_STM32H503

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello again,

I confirm both .cproject and .project files are missing in the repository.

Please paste the attached project files in the project folder root.

The github repo will be updated accordingly.

Thank you for raising the issue.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

7 REPLIES 7
KnarfB
Super User

There are no project files/folders

 .cproject
.mxproject
.project
.settings/

committed in that repo 

As a workaround, you may re-generate the project files by opening the .ioc in STM32CubeMX and generate code.

I have added stm32-hotspot to the title of your post. Maybe @Peter BENSCH can assist.

hth

KnarfB

Peter BENSCH
ST Employee

I would be happy to help - if I could and had enough time available. However, it should also be noted that it is not an officially supported project and as a project from the STM32 Hotspot, it is only intended to serve as a suggestion:

These materials are contributed by ST’s STM32 experts on an informal basis and may bring added value to users looking for additional STM32 software resources coming from a trusted source. As informal contributions, these materials are not officially produced, maintained, or supported by ST. Individual ST contributors may informally respond to questions and issues on a case by case basis at their discretion. Please check the CONTRIBUTING.md file included in each repository for more details. Due to the unofficial nature of materials in this STM32 Hotspot GitHub organization, user contributions are not accepted.

But maybe there is someone here who has already gained experience with it.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mƎALLEm
ST Employee

Hello @Anirudhoruganti ,

Could you please clarify what do you mean by "not able to import"? what are the steps you followed? do you have a compilation error? using STM32CubeIDE?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
mƎALLEm
ST Employee

Hello again,

I confirm both .cproject and .project files are missing in the repository.

Please paste the attached project files in the project folder root.

The github repo will be updated accordingly.

Thank you for raising the issue.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Anirudhoruganti
Associate II

The zip file is empty. 

I've downloaded the zip file and it contains both project files. 

And following is the content:

mALLEm_0-1748022436160.png

Please check again.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

It could be that the files starting with character . are hidden in the machine of @Anirudhoruganti.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.