cancel
Showing results for 
Search instead for 
Did you mean: 

Why is the "import cmake project" feature missing in the pre-release version?

newton_1232131
Associate

 

newton_1232131_1-1748496807933.pngnewton_1232131_2-1748496819935.png

Without this feature, you can't generate task files and launch files with one click like before to handle code downloading and debugging. Now you have to write the configurations yourself—it's just way too much hassle!

1 ACCEPTED SOLUTION

Accepted Solutions
Cartu38 OpenDev
Lead III
3 REPLIES 3
Cartu38 OpenDev
Lead III

Answers to your questionmarks are here 

https://www.youtube.com/watch?v=aWMni01XGeI

Cartu38 OpenDev
Lead III

About launch this one is auto generated if pushing Run & Debug button but not stored.
You can ask to "create a launch file" if you want to get it. It allows then much more options and control over your debug session. Tips: once .json open let's play with editor completion features ... a bit of teasing about done within this extension walkthrough 

Cartu38OpenDev_0-1748527561470.pngCartu38OpenDev_1-1748527593844.png