cancel
Showing results for 
Search instead for 
Did you mean: 

Ultra librarian creates erroneous symbols for STM32F4xxR2 in KiCAD 5 format

divmstr
Associate

I have the latest and greatest CubeIDE v1.16t.1, confirmed with recent attempts to upgrade it. Recently I have been experimenting with the ultra librarian tool output in the IOC editor, which looks to be extremely useful. I have a project that uses an STM32F401RBTX, it was created by an earlier version of CubeIDE, but upgraded when I opened it.

I use KiCAD 5, and have been able to successfully create a symbol on a different project. However, the symbol that it creates for this one has two errors: first the pins are all located on top of each other, and second the poly lines have fractional positioning data that is rejected by the symbol parser. I have attempted to text edit out the fractions, but the pins appear to be stuck together and any attempt to relocate them with the symbol editor fails. 

I cannot find any information about how to configure the librarian, is there an update or fix for this? Generated zip file is attached.

2 REPLIES 2
Ghofrane GSOURI
ST Employee

Hello @divmstr 

First let me thank you for posting.

This is a known issue that has been tracked by the ticket number  196222 

I will keep you posted with updates.

THX

Ghofrane 

Thanks. Is there any work-around? I tried a different project with an STM32F723, and it worked. (Except the symbol was rather large...)

 

Cheers