cancel
Showing results for 
Search instead for 
Did you mean: 

UART2 GPRS Communication Issue – Continuous Interrupts & Random Data

pankajprasad100
Visitor

Hello,

I'm currently working on an STM32 project using FreeRTOS, and I'm facing an issue with UART2 communication when interfacing with a GPRS module.

Project Setup:

  • UART3 is used for debugging (connected to a PC terminal) and is functioning correctly.

  • UART2 is used for communication with a GPRS module.

  • Both UART2 and the GPRS module operate at 3.3V logic levels.

  • The firmware uses STM32Cube HAL drivers and FreeRTOS.

What I’ve Verified:

  • The GPRS module was tested by connecting it directly to a PC using a USB-to-Serial converter, and it responds correctly to AT commands.

  • I also performed a loopback test on UART2 (connecting TX to RX), and it worked as expected — transmitted data was received correctly.

Issue Faced:

However, when I connect the GPRS module to UART2 (TX to RX, RX to TX, GND to GND), I observe that:

  • The UART2 interrupt triggers continuously, even when nothing is being sent.

  • The receive buffer fills with random or garbage data.

  • As a result, I’m unable to communicate with the GPRS module properly.

Questions:

  1. What could be the cause of continuous UART interrupts with invalid data?

  2. Are there any specific UART configurations or precautions when using external modules under RTOS?

  3. Could this be related to electrical noise, grounding, or missing hardware flow control (RTS/CTS)?

Additional Details:

  • STM32 MCU:STM32H755ZIT6U

  • Baud rate: 115200

  • UART2 is initialized through STM32CubeMX

Please let me know if you need any further details or if there’s a recommended way to debug this kind of issue.

Please look into my project and screenshots and I am using CM7 core.

Looking forward to your support.

1 REPLY 1
Andrew Neil
Super User

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results.

In particular, please give details of your hardware setup - used board(s), etc - your tool versions, etc

 


@pankajprasad100 wrote:
  • The GPRS module was tested by connecting it directly to a PC using a USB-to-Serial converter, and it responds correctly to AT commands..


Excellent - always a good start.

So have you done the same with your STM32?

ie, can the STM32 reliably communicate with a PC terminal?

How have you verified that the UART baud rate is actually correct?

 


@pankajprasad100 wrote:

I connect the GPRS module to UART2 (TX to RX, RX to TX, GND to GND)

Are you sure that's correct?

Some modules require TX-to-TX, and RX-to-RX (DCE connection)

 


@pankajprasad100 wrote:

I observe that:

  • The UART2 interrupt triggers continuously, even when nothing is being sent.

  • The receive buffer fills with random or garbage data.


Have you looked at the signals on an oscilloscope?

Have you used a USB-to-UART converter (or two) to "sniff" what's actually happening on the lines?

See:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/tac-p/706966/highlight/true#M49:~:text=some%20tips%20specifically%20on%20Debugging%20Serial%20Comms

 

PS:

 


@pankajprasad100 wrote:
  • I also performed a loopback test on UART2 (connecting TX to RX), and it worked as expected — transmitted data was received correctly..


Note that this test will pass even if the baud rate is not what you think it should be.

 

Have you got reliable comms working between STM32 & GPRS unit without the RTOS ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.