cancel
Showing results for 
Search instead for 
Did you mean: 

SystemInit, SystemCoreClock and AHBPrescTable suddenly undefined?

Robert Poor
Associate III

I built a project for the NUCLLEO-G431RB using STM32CubeIDE v 1.9.0. Somewhere along the line, it offered to upgrade to 1.10.0 which I accepted, and it also warned that my ws was tied to an older version, for which I opted to upgrade the ws. (Either of those might have been a mistake!)

But now my build fails with SystemInit, SystemCoreClock and AHBPrescTable showing as undefined. I'm not sure where along the line it happened, but how do I get them back into the project?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Robert Poor
Associate III

Half solved:

I created a new project for the NUCLEO-G431RB, searched for SystemInit and found it in Core/Src/system_stm32g4xx.c. I copied that into the failing project and -- lo and behold -- it worked.

What I don't know is what caused system_stm32g4xx.c to vanish in the first place.

Markus GIRDLAND
ST Employee

Hello Robert,

I believe this issue could be related to the regression introduced in STM32CubeIDE 1.10.0. It was mentioned on the community here.

Moving to STM32CubeIDE 1.10.1 should solve the issue.