2023-12-05 2:11 AM
Hello,
A few days ago I compiled on my STM32l562E-DK board the TFM application (which includes TFM_SBSFU_Boot, TFM_Loader, TFM_Appli) of STM32Cube_FW_L5_V1.5.0 package. After that I experienced some errors. The first one was DEV_TARGET_NOT_HALTED which I managed to solve by doing a boot from RSS. Then, I tried debugging the example project “GPIO_IOToggle_TrustZone_Secure” and I got the second error: “No source available for <signal handler called>() at 0xfffffffe” and “failed to execute MI command. Error message from debugger back end: Cannot access memory at ...“.
This happens with any TrustZone enabled project I try to debug.
I would appreciate any tip or assistance. Than you in advance!
2023-12-05 5:23 AM
Hello @Claudia,
First let me thank you for posting and welcome to the ST Community.
Your request is under investigation, and I will get back to you ASAP.
Thanks.
Mahmoud.
2023-12-15 2:40 AM
Hello @Claudia ,
I escalated the problem to CubeIDE team in an internal ticket (ID: 163832) to take a closer look at this issue.
(PS: ID 163832 is an internal tracking number and is not accessible or usable by customers).
Thanks.
Mahmoud.
2024-01-11 4:33 AM
Hello,
Any news on my issue?
Thank you in advance,
Claudia.
2024-03-27 11:32 PM - edited 2024-03-28 1:05 AM