STM32CubeIDE Silent/Noninteractive Install
I'm attempting to set up a CI pipeline to build firmware built in STM32CubeIDE, but I've not been able to get STM32CubeIDE installed via Dockerfile without manual intervention. Is there a silent install or a way to pre-accept the license agreements so that I can install the STM32 toolchain without having to hand-build my Docker images?
The container base is Ubuntu 22.04. I've tried piping `yes` to to the installer, as well as `expect` and `printf`, but the license script fails when run any way other than the default. Similarly, I've tried extracting the .debs from the script and installing via `apt` with the same results. I'm not trying to circumvent the license, I just want a way to set up the tools in a Docker container without manual intervention.