2025-03-11 4:37 AM
I'm using STM32f407 board with Cubeide. When load new code, I want to work code after pressing reset button.
How can I set it in STM32CubeIde.
Thank's
2025-03-11 5:14 AM
If this is a custom board, ensure BOOT0 is pulled down.
Use the standard linker file that uploads to flash.