cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE opens on non-present screen.

Andrew Neil
Super User

Win 11 Laptop with external (large) monitor.

When the laptop is then used without the external monitor, apps should open on the internal one.

Most do; STM32CubeIDE (v1.13.0) doesn't - it still positions itself as it the non-connected screen were still there.


Addendum

If you get stuck in this situation, the IDE window can be retrieved by:

  1. Give the IDE window focus (eg, Alt+TAB to it)
  2. Press Alt+Spacebar.
    The window control menu will appear at the edge of the real screen:
    AndrewNeil_0-1709311291831.png

     

  3. Select 'Move'.
    The cursor keys will now move the IDE window - use them to move it onto the real screen.
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
0 REPLIES 0