cancel
Showing results for 
Search instead for 
Did you mean: 

STM32cubeIDE make: [makefile:103: STM32H747I-DISCO_CM7.elf] Error 127

judy
Associate II

11:06:38 **** Incremental Build of configuration Debug for project STM32H747I-DISCO_CM7 ****

make all

arm-none-eabi-arm-none-eabi-arm-none-eabi-gcc -o "STM32H747I-DISCO_CM7.elf" @"objects.list" -l:libtouchgfx-float-abi-hard.a -mcpu=cortex-m7 -T"G:\TouchGFX\TouchGFXProjects\MyDemo\STM32CubeIDE\CM7\STM32H747XIHX_FLASH.ld" --specs=nosys.specs -Wl,-Map="STM32H747I-DISCO_CM7.map" -Wl,--gc-sections -static -L../../../CM7/Middlewares/ST/touchgfx/lib/core/cortex_m7/gcc --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group

g:/stm32cubeide_1.15.1/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.make.win32_2.1.300.202402091052/tools/bin/sh: arm-none-eabi-arm-none-eabi-arm-none-eabi-gcc: not found

make: *** [makefile:103: STM32H747I-DISCO_CM7.elf] Error 127

"make all" terminated with exit code 2. Build might be incomplete.

 

11:06:40 Build Failed. 1 errors, 0 warnings. (took 2s.517ms)

 

How to solve this problem?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Pavel A.
Super User

arm-none-eabi-arm-none-eabi-arm-none-eabi-gcc: not found

The ARM toolchain is not found. Check in the project properties that the toolchain is installed. If not - either install the needed toolchain or select one of available toolchains.

thanks,I solved the problem by regenerating the code with touchgfx, then configuring it with cubeMX, and then recompiling it in cubeIDE.