cancel
Showing results for 
Search instead for 
Did you mean: 

stm32cubeide freeRTOS task list update

yang hong
Associate II

I am using nucleo-f439zi in stm32cubeide with freertos debug. It seems everything is working, the only thing is that I need pause program if I would like to see freertos task list status. Is it possible to track task list status when system is running?

3 REPLIES 3
Sarra.S
ST Employee

Hello @yang hong,

 In stm32CubeIDE, the following views are available for FreeRTOS:

  • FreeRTOS Task List
  • FreeRTOS Timers
  • FreeRTOS Semaphores
  • FreeRTOS Queues

If the Run Time column in the FreeRTOS Task List view displays after making three settings

Please check the settings in paragraph 3.4.2.1.3 RTOS profiling information in UM2609

PS: the problem can arise if project is not built with an optimization level -O0

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I did all following manual instruction for FreeRTos, however, I still need suspend program to make FreeRTOS task list update. Is it true for this feature?

Ok, 

Finally, I got some explanation from manual.

 

yanghong_0-1713895125211.png

Frankly, I am little bit disappointed because stm32cubeide can't make task list view to update during the program running.