cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE depends on discrete GPU on macOS

XWang.5
Associate II

Hi Community,

The env is: STM32CubeIDE 1.8.0, macOS 10.15.7, MBP16-2019

When STM32CubeIDE is running, the OS switches to discrete GPU and eat about 30W totally(with integreted GPU only 10W is needed). The battery is running low fast.

I force switch to integreted GPU with gSwitch. Everything seems OK.

So would ST please check why STM32CubeIDE is designed to depends on discrete GPU on macOS? If it is not necessary, it would brings huge convenince to remove the dependency.

Thanks.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0