2024-12-28 03:39 PM
I changed an example program for STM32F4 Discovery Board to C++ project.
When compiling the project, there are files included from BSP, which includes a definition:
extern "C".
When compiling the project, the first error is the following:
../../Drivers/BSP/STM32F4-Discovery/stm32f4_discovery.h:25:9: error: expected unqualified-id before string constant
25 | extern "C" {
| ^~~
what is the problem?
Thanks for responsing
2024-12-29 09:30 AM
Any effort to prevent repeated inclusion of the same include file?
Closing brace matching?