2021-09-01 4:57 AM
2021-09-01 5:13 AM
For example on my system in c:\ST\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_1.6.0.202101291314\tools\bin\
i create config.txt and start persistent ST-LINK_gdbserver.bat , that i can connect from other world place over forwarded debug port...
2021-09-01 5:30 AM
I can"t find the option for changing address:
root@Debug-0:~# /usr/bin/stlink-server --help
stlink-server
--help | -h display this help
--version | -v display STLinkserver version
--port | -p set tcp listening port
--debug | -d set debug level <0-5> (incremental, 0: Error, 1:Info, 2:Warning, 3:STlink,
4:Debug, 5:Usb)
--auto-exit | -a exit() when there is no more client
--log-output | -l redirect log output to file <name>
2021-09-03 8:51 AM
Seems on windows works ok, but for linux limited to localhost?
C:\Users\spravca>netstat -na
Active Connections
Proto Local Address Foreign Address State
TCP 0.0.0.0:135 0.0.0.0:0 LISTENING
TCP 0.0.0.0:445 0.0.0.0:0 LISTENING
TCP 0.0.0.0:990 0.0.0.0:0 LISTENING
TCP 0.0.0.0:2869 0.0.0.0:0 LISTENING
TCP 0.0.0.0:5357 0.0.0.0:0 LISTENING
TCP 0.0.0.0:49152 0.0.0.0:0 LISTENING
TCP 0.0.0.0:49153 0.0.0.0:0 LISTENING
TCP 0.0.0.0:49154 0.0.0.0:0 LISTENING
TCP 0.0.0.0:49157 0.0.0.0:0 LISTENING
TCP 0.0.0.0:49158 0.0.0.0:0 LISTENING
TCP 0.0.0.0:50128 0.0.0.0:0 LISTENING
TCP 0.0.0.0:61234 0.0.0.0:0 LISTENINGSTMicroelectronics ST-LINK GDB server. Version 5.8.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Enabled
LogFile Name : debug.log
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Target connection mode: Default
Reading ROM table for AP 0 @0xe00fffd0
Hardware watchpoint supported by the target
COM frequency = 4000 kHz
ST-LINK Firmware version : V2J37M26
Device ID: 0x421
PC: 0x8000e38
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.25 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...