2025-09-13 9:45 AM
Building upon my previous post, "Bidirectional Serial Communication with ST-Link using FreeRTOS on NUCLEO Boards," this code demonstrates a Simulator component and an Application component operating on two separate NUCLEO-C092RC boards. Please note that this project is intended for educational use and is not designed as robust production code; some errors or omissions may remain that users will need to address. This initial demonstration should function as described when configured according to the provided instructions, and it may serve as a foundational template for future development and enhancements.
Val Gretchev