cancel
Showing results for 
Search instead for 
Did you mean: 

Sending position information from BissC absolute encoder to STM32F401 via SPI

aknaydn
Associate

Is it possible for BissC absolute encoder to communicate with STM32F401Re via SPI? Or can it be with MAX485 module as in the ardunio example in the link below? 

 

https://protonestiot.medium.com/communication-between-24-bit-rotary-encoder-working-with-biss-ssi-and-arduino-1a85c64b7262

0 REPLIES 0