SDMMC on H7 using CubeIDE 1.8.0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-13 2:51 PM
Has anyone else had problems with the SDMMC peripheral on the H7 since the CubeIDE 1.8.0 Update. I have some old projects I went back to that had previously used this peripheral and now when mounting the SD Card I get a FR_NO_FILESYSTEM error. I have also started from scratch with a new project and ran into the same error.
I looked into this thread as well:
https://community.st.com/s/question/0D53W00000cShQ1SAK/stm32h735-sdmmc-error-frnofilesys
but it looked to me like they removed the ENABLE_SD_DMA_CACHE_MAINTENANCE define.
My general setup comes from the tutorial put out by ST:
https://www.youtube.com/watch?v=I9KDN1o6924
Also everything for the SD Card is in the D1 Ram and I am not using FreeRTOS
Am I missing something with weird H7 memory? Or could the update have messed up this peripheral?
- Labels:
-
SDIO-SDMMC
-
STM32CubeIDE
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-13 4:19 PM
Looking at the logic analyzer from test on the old project this is the expected communication protocol
Currently I am now seeing this communication
It seemed odd to me to see so much movement on the card detect line.
There are currently internal pullups (through the CubeMX) on each of the data lines and the Card Detect line.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-12-14 9:21 AM
Ended up being a signal integrity issue. Changing Pull-Ups from internal in CubeMX to external Pull-Ups on my circuit fixed the issue.
The SD Card was working for about 20-30 program cycles and then went back to the state of always returning FR_NO_FILESYSTEM. Any ideas of what could be going wrong?
My SDMMC Clock is 6MHz (240MHz/(20MHz*2)) coming from the PLLQ1. Heap Size: 0x400 and Stack Size: 0x800. ICache and DCache are disabled.