cancel
Showing results for 
Search instead for 
Did you mean: 

PWM Output on PB0 and PA8 does not Reach 0V or 3.3V (STM32F429I-Discovery)

chachamaru
Associate III

Hello,

I am currently wor

king on connecting an MT9M001 camera module to the STM32F429I-Discovery board and displaying the captured image on a PC.
During this process, I am testing PWM output on the board, but I am experiencing an issue where the output voltage does not swing between 0 V and 3.3 V as expected.

Environment

  • Board: STM32F429I-Discovery

  • IDE / Firmware: STM32CubeIDE + HAL (STM32CubeF4 package)

  • Pin used: PB0 / TIM3_CH3 (Alternate Function, Push-Pull, no pull-up/down)

  • PWM: Generated with TIM3 (frequency and duty cycle shown in attached code/images)

  • Measurement: Oscilloscope (×10 probe, GND connected to board GND)

Issue

The PWM waveform output from PB0 shows the following problems:

  • The low level does not go down to 0 V

  • The high level does not reach 3.3 V

Before switching to PB0, I was using PA8 (TIM1_CH1), but I observed the same issue—
the voltage could not drop to 0 V.
I received advice that PA8 might be loaded by other on-board circuitry,
so I moved the PWM output to PB0 (TIM3_CH3).
However, the same reduced voltage swing occurs on PB0 as well.

If anyone knows possible causes or has experienced a similar issue,
I would appreciate any guidance.

TEK00016.PNG

0 REPLIES 0