cancel
Showing results for 
Search instead for 
Did you mean: 

Put 'mx.scratch' under source control?

StefanRickli
Associate II

After generating code for a migrated project (from TrueStudio & CubeMX), I noticed a new file 'mx.scratch' in the project's root.

Is this a temp file that gets generated from other files or shall I take it under source control?

2 REPLIES 2
Cartu38 OpenDev
Lead II

Yes such file is a temp file. If regular behavior you should see it only during CubeMX project generation process. If getting it by the end of the process most probably some unexpected issue happens in between.

StefanRickli
Associate II

I just reran code generation and 'mx.scratch' doesn't get deleted after it's done. But I don't get any error messages, and the produced code looks fine.

Is there a log somewhere that I can consult?