2019-12-07 3:48 PM
Hi all,
Afer copy/paste of project cubemx .ioc file name is not updated accordingly and cannot be opened.
Manual updating name of .ioc file is fixing this issue.
Regards,
Pawel
Solved! Go to Solution.
2019-12-09 4:32 AM
Ok, so you copy through the Project Explorer inside CubeIDE?
I see that it doesn't change name of ioc and content of ioc points to old project as well.
I'll write a ticket for it!
2019-12-09 1:49 AM
Just so I understand it correctly:
If you have the project:
C:/workspace/myProject
Then you copy it in Windows it will rename it to:
C:/workspace/myProject - Copy
But the .ioc file is still pointing towards C:/workspace/myProject and any change made will be made towards that project when you generate code etc.
And that's what this issue is about, right?
2019-12-09 3:26 AM
Im using Ubuntu, but copy/past it is basic Eclipse function.
To reproduce click in CubeIDE right mouse button over the project and then Copy and again Past.
Project is copied but ioc file stli is pointing to previous project name and when you try to open it it says:
Invalid Input: Must be project's active .ioc file.
Project's 'App_test001' active one is 'App_test001.ioc' file
Then ioc file in project has name App_test000.ioc.
During project copying ioc file should be renamed inline with project.
Regards,
Pawel
2019-12-09 4:32 AM
Ok, so you copy through the Project Explorer inside CubeIDE?
I see that it doesn't change name of ioc and content of ioc points to old project as well.
I'll write a ticket for it!
2019-12-09 5:46 AM
Thank you Markus,
My other wish is option to save SWO output to file or some other possibility to have acces to SWO.
https://community.st.com/s/question/0D50X0000BcR3uwSQC/save-swo-to-file
Why?
Segger support for stm32g4 is shaky and I moved to smt32cubeIDE but here I'm lack RTT tools.
At the moment I try to write RTT using openOCD but here another problem is that support for STlink3 is not great (https://sourceforge.net/p/openocd/tickets/259/)
Regards,
Pawel
Regards,
Pawel
2019-12-09 11:39 PM
Those signatures seem to do more harm than help...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.