2023-06-22 05:48 AM
After an update i am not able to debug my program. I have already tried an new installation of the STMCubeIDE 1.12.0 but it still doesn't work. I've already tried to add a local toolchain in the Toolchain Manager, but the error still apears. Does anybody have an idea to solve this problem?
2023-06-22 06:47 AM
Hello @Stone1234
First let me thank you for posting.
I suggests you to start by locating the GDB Server
It is possible that anti-virus software has either deleted gdb or prevented it from launching. Test 1&2 should be sufficient to tell you if this is true…
I will wait for your feedback.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-06-22 11:08 PM
Hello CHERNI,
thank you for the quick reply.
I executed the steps 1 & 2 and got this as the result from cmd:
2023-06-27 06:01 AM
Same here. It works once as soon as I restart STM32CubeIDE and plug the Nucleo board usb cable. Then it stops working. I've just updated the ST-Link firmware on the Nucleo board to latest version.
2023-06-30 01:04 AM
2023-07-05 03:48 AM
@Semer CHERNIAbove, you see the .log file.
2023-08-30 01:07 AM
now I face the same problem with 1.13.1.
for my case, no problem last week, but met error in this week, so I tried clean install with new PC setup yesterday, and also get same error today on new PC.
Attached log file shows following activities..
SESSION 2023-08-29 16:47:02.951
-- inport 2 project from other PC, and do some Debug without problem.
SESSION 2023-08-30 08:29:33.942
-- to make merge from 2 projects, copy one and paste to new-named project, then quit IDE.
SESSION 2023-08-30 08:54:45.200
-- after making merge into new project (using external merge tool), then start IDE and get error when Run/Debug.
further detailed infos, please refer .xlsx attached but sorry that is in Japanese.
still in need help...