cancel
Showing results for 
Search instead for 
Did you mean: 

Neu build Error when using STM32CubeIDE1.15.0

JPan.4
Associate III

Version: STM32CubeIDE1.15.0

 

Hallo ST community,

due to the project-related reason, I need to use an old compile toolchain com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.1.100.202309262110 . So I download this toolchain and specify it as my fix toolchain in the toolchain manager. I got then the following error whild compiling:

 

 

arm-none-eabi-objdump -h -S MoreDisplay.elf  > "MoreDisplay.list"
arm-none-eabi-objcopy  -O ihex MoreDisplay.elf  "MoreDisplay.hex"
   text	   data	    bss	    dec	    hex	filename
4805660	    384	 901644	5707688	 5717a8	MoreDisplay.elf
c:/st/stm32cubeide_1.15.0/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.make.win32_2.1.300.202402091052/tools/bin/sh: arm-none-eabi-objdump: not found
make: *** [makefile:114: MoreDisplay.list] Error 127
make: *** Waiting for unfinished jobs....
c:/st/stm32cubeide_1.15.0/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.make.win32_2.1.300.202402091052/tools/bin/sh: arm-none-eabi-objcopy: not found
make: *** [makefile:119: MoreDisplay.hex] Error 127

 

 

After investigating the folder, there are indeed no  arm-none-eabi-objdump and objcopy files. 

Actually, that is the point which makes me confused. I have already specified my fix toolchain, why the new IDE still want to use these two files from other extern tools? These two files exits in my fix old toolchain.

In the older version of IDE V1.14.0, it has no problem with the fix old toolchain.

 

Thanks for your help!

 

Best wishes

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0