cancel
Showing results for 
Search instead for 
Did you mean: 

Live expressions not working properly

AVill.1
Associate II

I am atrying to look at some global variables while debugging using the live expression feature, but when I add them and run the program I can only see a blank space that some times is filled by a 0. It is like flashing sometimes,

I have checked my debugger options and I think that I have them properly set.

0693W00000FBjwvQAD.png

1 REPLY 1
TDK
Guru

Works for me.

What variables are you trying to watch? Are the declared globally?

Perhaps a screenshot would help describe the issue.

Is "0" the value you expect for the variable?

If you feel a post has answered your question, please click "Accept as Solution".