cancel
Showing results for 
Search instead for 
Did you mean: 

Latest STM32CUBE IDE problems. Malloc() failure.

DavidAlfa
Senior II

I upgraded to STM32CUBE IDE v1.5 few days ago, then strange problems began to appear.

Suddenly, code that previously worked on v1.3, doesn't. No major changes.

The program uses a some dynamic memory allocation, so to debug the free memory, I use this routine.

It allocates adding 100 byte blocks. I know it's not perfect, but it gives me a idea of the memory usage.

It worked well last time I used it, 2 weeks ago, allocating 10K of ram before and 2K after the program initialization.

Now the malloc always returns a valid pointer, and the allocation value increases without control until it triggers a HardFault.

__attribute__((optimize("O0")))	// Disable all optimizations
uint16_t freeram(void){
  uint16_t ram=100;		// Start with 100 byte allocation
  uint8_t* ptr;			// Pointer for malloc function
    while(1){
      ptr=malloc(ram);		// Try to malloc 'ram' bytes
      if(ptr==NULL){		// If null pointer
        return (ram-100);	// Return previous ram value
      }
      else{			// If not null
        free(ptr);		// Free up the allocated memory
        ram+=100;		// Increase allocation size
      }
    }
}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0