cancel
Showing results for 
Search instead for 
Did you mean: 

Issues when generating a ML inference project for the Nucleo STM32N657

edupuis
Associate

Dear ST community,

I'm trying to setup a ML inference project on the STM32N6 Nucleo in order to do latency and accuracy evaluation of models as well as power measurements. I've been stuck at setting up a project that builds for a few days now.

  • Environment:

    • Nucleo STM32N657 X0h3Qu
    • ST CubeIDE 1.18

    • X-Cube-AI 10.0.0

  • From CubeIDE create new project

    • File -> New -> STM32 Project

    • Select N6 Nucleo board

    • Name=N6_Test_02, Target language=C, Project structure=Secure and Non secure domain, FSBL only

  • In the embedded cubeMX, Add X-Cube-AI and add my model

    • Pinout & Configuration -> X-CUBE-AI

    • Select context FSBL, check X-Cube-AI -> Core and select device application application template, hit ok

    • Pinout & Configuration -> X-CUBE-AI -> Add network TFLITE, Neural Art runtime, select my custom model, Analyze, model fits on device (800Kb Flash, 125KB RAM)

  • Fix the clock configuration manually

    • CPU clock MUX SYSA is said to have 600Mhz max although the IC1 source is selected and in the PLL1, I can see that the IC1 has a /2 divider and 800Mhz , at this stage select /1 then select back /2 fix the issue, SYSA gets the desired 800Mhz and the warning disappear
  • Save and generate the code

  • Fix the missing aton library

    • Build the FSBL -> ../X-CUBE-AI/App/network.c:46:10: fatal error: ll_aton_NN_interface.h: No such file or directory

    • Copy files and folder from /home/%USER/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/10.0.0/Middlewares to the FSBL

    • Add /N6_Test_02_FSBL/Middlewares/ST/AI/Npu/ll_aton and /N6_Test_02_FSBL/Middlewares/ST/AI/Npu/Devices/STM32N6XX to the include path

  • Fix the RIF_RISC_PERIPH_INDEX_NPU issue

    • Build the FSBL -> ../X-CUBE-AI/App/app_x-cube-ai.c:100:43: error: 'RIF_RISC_PERIPH_INDEX_NPU' undeclared (first use in this function)

    • From the project top level, move everything in Drivers in the Drivers view of the project, Add the includes /N6_Test_02_FSBL/Drivers/STM32N6xx_HAL_Driver/Inc, /N6_Test_02_FSBL/Drivers/CMSIS/Device/ST/STM32N6xx/Include, /N6_Test_02_FSBL/Drivers/CMSIS/Include, /N6_Test_02_FSBL/Drivers/BSP/STM32N6xx_Nucleo

    • Copy /home/$USER/STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/10.0.0/Projects/STM32N6570-DK/Applications/hello_world/Drivers/STM32N6xx_HAL_Driver/Inc/stm32n6xx_hal_rif.h (and .c ) to /N6_Test_02_FSBL/Drivers/STM32N6xx_HAL_Driver/Inc (/Src for the .c)

    • Add NPU_PRESENT to the preprocessor

    • Add #include "stm32n6xx_hal_rif.h" Line 46 of /N6_Test_02_FSBL/X-CUBE-AI/App/app_x-cube-ai.c

  • Fix the make: *** No rule to make target '/work/PSEE/stm32_2/N6_Test_02/Drivers/BSP/STM32N6xx_Nucleo/stm32n6xx_nucleo.c', needed by 'Drivers/BSP/STM32N6xx_Nucleo/stm32n6xx_nucleo.o'. Stop. issue



    I'm stuck at the last issue mentioned.

    any help would be appreciated,

    Thanks,
    Etienne
0 REPLIES 0