2021-03-27 12:23 PM
I am running the STMCubeIDE 1.5.1 and would like to debug two boards simultaneously. One is a NUCLEO-H723ZG and the other is a NUCLEO-F303RT. The applications for each are designed to communicate with each other through the SPI ports on each. So I would like to debug the communication protocol between the two boards.
I can detect the unique serial numbers of each board under Debug Configurations > Debugger > ST-LINK S/N pull down menu after pressing the SCAN button. For the first debug session, I have checked Autostart local GDB server, but for the second I have checked Connect to remote GDB server instead because restarting the server upon launching the second session results an a GDB server error. What is the correct configuration for each debug session, provided that this is even possible?
Solved! Go to Solution.
2021-03-28 10:28 AM
You can open two instances of STMCubeIDE, one for each board and use the serial numbers of either ST-LINK.
2021-03-28 10:28 AM
You can open two instances of STMCubeIDE, one for each board and use the serial numbers of either ST-LINK.
2021-03-30 4:11 AM
Or rely on same IDE session but enjoy STlink server feature (openOCD and GDB server compliant):
Just "assign" each debug configuration to targetted board.
Connected device limit is USB port enumeration limit.