cancel
Showing results for 
Search instead for 
Did you mean: 

Invalid Input: Must be project's active .ioc file.

MStre.1
Associate II

Hi,

i want to clone my project. I did the following steps:

1) Edit > Copy.

2) Edit > Paste.

3) Rename the ioc files.

4) Delete the Debug.launch file.

5) Project > Clean.

the next step is to generate the CubeMX. But when I try to open the .ioc file this error message occurs:

Invalid Input: Must be project's active .ioc file.

can anybody help me please?

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11

Hi Peter,

I opened the project with the newest STM32CubeIDE and migrated it to the newest firmware.

It works and I can open the .IOC file now after copy and paste the project.

Thanks for your help Peter!

Peter BENSCH
ST Employee

Great!

If the problem is solved, please mark this thread as answered by selecting Accept as Solution, as also explained here. This will help other users find that answer faster.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.