‎2019-12-21 06:22 AM
Installing STM32CubeMx on OpenSuse Tumbleweed using
/st-stm32cubeide_1.1.0_4551_20191014_1140_amd64.rpm_bundle.s
is missing libusbx
sudo ./st-stm32cubeide_1.1.0_4551_20191014_1140_amd64.rpm_bundle.sh
[sudo] Passwort für root:
Creating directory st-stm32cubeide_1.1.0_4551_20191014_1140_amd64.rpm_bundle.sh.root
Verifying archive integrity... All good.
Uncompressing STM32CubeIDE installer 100%
Verifying... ################################# [100%]
Preparing... ################################# [100%]
package segger-jlink-udev-rules-6.44c-4.noarch is already installed
error: Failed dependencies:
libusbx >= 1.0 is needed by st-stlink-server-1.2.0-3.amd64
Verifying... ################################# [100%]
Preparing... ################################# [100%]
package st-stlink-udev-rules-1.0.2-2.noarch is already installed
error: Failed dependencies:
st-stlink-server is needed by st-stm32cubeide_1.1.0-1.1.0-4551_20191014_1140.x86_64
libusbx is not available for OpenSuse. On https://sourceforge.net/projects/libusbx/
SourceForge: libusbx is OBSOLETE and has been superseded by http://libusb.info
What can I do?
‎2023-02-02 02:48 AM
So I got it to install. I used the generic installer, opened with Sudo and allowed it to ignore the dependencies. At the licence pressing q then y works.
​
I have attempted one hello world but it doesn't seem to compile so I'll fight for another few days or just spin up win-doze on a VM
‎2023-02-02 04:01 AM
This is the situation with Linux. Linux is free. CubeIDE is free too. Your time and effort has price. You decide whether it's worth it.
‎2023-02-02 05:13 AM
😊
‎2023-02-02 09:45 AM
rpm package asks for yum to install
License accepted.
error: Failed dependencies:
libusbx >= 1.0 is needed by st-stlink-server-2.1.0-1.x86_64
Verifying... ################################# [100%]
Preparing... ################################# [100%]
package st-stlink-udev-rules-1.0.3-2.x86_64 is already installed
./setup.sh: Zeile 21: yum: Kommando nicht gefunden.
./setup.sh: Zeile 21: yum: Kommando nicht gefunden.
still the libusbx dependenci
‎2023-02-02 09:56 AM
st-stm32cubeide_1.11.2_14494_20230119_0724.unsigned_amd64.sh
installs the software and starts correct.
May be libusb is missing later when trying to connect to segger
‎2023-02-02 10:40 AM
Windows and MacOS are free too Pavel so I'm not sure you understand the ecosystem very well. Thank you for your helpful comment though.