cancel
Showing results for 
Search instead for 
Did you mean: 

I installedCubeIDE and have the NUCLEO L476RG board connected. It contains the default program and is responding to User button. I do not see src folder on left and do not know how to save and get started. Please help

TMuth.2
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
MM..1
Chief III

Simply setup and manage all GPIO and peripherals in ioc window and close ioc. On closing code is generated for you and in Core left can select... open files...

View solution in original post

4 REPLIES 4
MM..1
Chief III

Simply setup and manage all GPIO and peripherals in ioc window and close ioc. On closing code is generated for you and in Core left can select... open files...

TDK
Super User

There are source files within the Core folder.

If you feel a post has answered your question, please click "Accept as Solution".

Thanks @TDK​. I am able to locate the source files

Thanks @MM..1​ . That helped