cancel
Showing results for 
Search instead for 
Did you mean: 

How to delete old .launch files

STuser2
Senior III

Whenever i rename a project. launch file is created and a number of. launch files are generated for each project name, is it possible that automatically that the old launch files are deleted, i can delete manually but just checking if it can be deleted automatically as soon i rename the project. 

1 ACCEPTED SOLUTION

Accepted Solutions
Semer CHERNI
ST Employee

Hello @STuser2 

First let me thank you for posting.

The launch file take it's name from the debug Debug Session name:

SemerCHERNI_0-1752058279961.png

Also to delete the launch file you just delete the debug configuration having the same name.

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
KnarfB
Super User

Haven't seen any automatic delete on renaming. In fact, one can have several launch files for different configurations, so there is not necessarily a 1:1 relation between .lauch name(s) and project name.

hth

KnarfB

Semer CHERNI
ST Employee

Hello @STuser2 

First let me thank you for posting.

The launch file take it's name from the debug Debug Session name:

SemerCHERNI_0-1752058279961.png

Also to delete the launch file you just delete the debug configuration having the same name.

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.