2022-04-29 6:20 AM
Greetings!
I'm using this printf library: https://github.com/mpaland/printf
And would like to completely disable the printf in the C Libraries that come with STM32CubeIDE. I went as far as renaming my printf to DBG, but when I look in the map file there is still printf included from the library. Here is an example:
.text._vfprintf_r
0x000000000800dc4c 0x260 c:/st/stm32cubeide_1.7.0/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+dp/hard\libc_nano.a(lib_a-nano-vfprintf.o)
0x000000000800dc4c _vfprintf_r
0x000000000800dc4c _vfiprintf_r
.text._printf_common
0x000000000800deac 0xda c:/st/stm32cubeide_1.7.0/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+dp/hard\libc_nano.a(lib_a-nano-vfprintf_i.o)
0x000000000800deac _printf_common
*fill* 0x000000000800df86 0x2
.text._printf_i
0x000000000800df88 0x24c c:/st/stm32cubeide_1.7.0/stm32cubeide/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+dp/hard\libc_nano.a(lib_a-nano-vfprintf_i.o)
0x000000000800df88 _printf_i
Is there anyway to get rid of this extra code that I just do not want to use?
Thank you!
2022-04-29 7:17 AM
Not sure, but if I don't use printf, it doesn't appear in the map file. Are you sure it's not being used somewhere in the program? Is the replacement printf include appearing before all instances of printf?
There is this checkbox, but it had no effect for me when I tried it with printf.
As a note, I use the same printf replacement in my code. It works well.
2022-04-29 7:24 AM
That box is checked.
I did a global search for "printf" and don't see anything in the project other than things like vsnprintf_ that is in the third party library I mentioned.
I would have thought this would be trivial fix. I don't see a way to disable the nano lib, seems like it gets included in some form.
Thanks for your response.
2022-04-29 7:26 AM
I guess technically you need to look for "printf_". If that's not in your map file, your program is not using the replacement printf library.
2022-04-29 7:30 AM
I had renamed the function to DBG and that is in the map file. I can trace into it with the debugger too. So i know that is being used.
2023-08-04 3:03 PM
Was there any resolution to this? Anyway to disable the built in printf libraries to guarantee our own is being used?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.