cancel
Showing results for 
Search instead for 
Did you mean: 

how do i change the driver?

Psang.2
Associate II

I'm using NUCLEO-207FZG

In cubeIDE, HAL driver is provided by default.

I want to change to the SPL(Standard Peripheral Library).

Since I am a beginner, I would like to get tips. Before you try, ask a question.

I wonder if it is enough to simply add the SPL folder, or if there is a function to change the library in cubeIDE?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
S.Ma
Principal

As spl is deprecated, it should be considered user code for the STM32Cube SW tools

View solution in original post

2 REPLIES 2
S.Ma
Principal

As spl is deprecated, it should be considered user code for the STM32Cube SW tools

Thank you :)