cancel
Showing results for 
Search instead for 
Did you mean: 

How do I build STM32CubeIDE project(s) using the command line and a continuous integration engine?

PSand.1052
Associate

I have to build some projects that were developed in STM32CubeIDE using a continuous integration engine. This involves checking out the Git repo containing a project, then issuing commands to generate the Makefiles and make the relevant targets. This is a C++ project using the Gnu Make builder, and the build host is headless.

The help center offers no insight into this, an Internet search was not helpful, and I could not find a mention of continuous integration in the ST communities.

What command(s) should I issue to generate the project's Makefiles?

Many thanks in advance,

Paul

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Tom V
Associate

My build server runs a command like:

/opt/st/stm32cubeide_1.1.0/stm32cubeide --launcher.suppressErrors -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data workspace -import demo -cleanBuild demo/DebugBuild

GreenGuy
Lead

I am running 1.3.0 in linux LMint version 19.3 and the answer given does not work. Perhaps somethings have changed since the IDE version 1.1.0.

Tom V can you point to where you obtained the information that lead to the command line you use?

Check headless.sh in the same directory with CubeIDE executable

-- pa