cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, How to use/connect STM32CubeIDE with Nucleo144-H7 board? I've installed STM32CubeIDE, STM32CubeMX, STM32CobeProgrammer and STLink (Server) under Ubuntu Linux. I get an error when I try to download and debug (see attachment)! Can anybody help me?

Mick P. F.
Senior
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Mick P. F.
Senior

Hello Markus,

I've already solved this problem. I missed a right manual, I could not find it at the STM site, but I found it anywhere in the internet few days ago: I have to connect the board via "User USB" to program access/program the flash! Now it works.

Sometimes it is very useful to have access to and to read the manuals.

Kind Regards,

Michael

View solution in original post

2 REPLIES 2
Markus GIRDLAND
ST Employee

Is this for any project you create or for this specific one?

Can you connect to the board if you're using the stand-alone CubeProgrammer? Available here.

Mick P. F.
Senior

Hello Markus,

I've already solved this problem. I missed a right manual, I could not find it at the STM site, but I found it anywhere in the internet few days ago: I have to connect the board via "User USB" to program access/program the flash! Now it works.

Sometimes it is very useful to have access to and to read the manuals.

Kind Regards,

Michael