cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I got some procompiled .o files (Atollic studio) for my CubeIDE Project. In which way can i include this files. Best regards Stephan

SHung.140
Associate
 
2 REPLIES 2
turboscrew
Senior III

You compile your code with header files that contain the definitions of the global symbols of the object files, and then link the object files with the program.

Ozone
Lead III

You can use the ranlib tool to create a library. It is usually part of the gcc toolchain.

And yes, you would need the headers for the compiler.