2022-05-10 1:57 AM
2022-05-12 4:14 AM
#define ElemanSayisi 1000
uint8_t buffer[ElemanSayisi] =
{ 6, 4, 0, 7, 7, 1, 7, 6, 5, 3, 1, 3, 3, 0, 6, 2, 4, 9, 1, 9, 2, 2, 5,
1, 1, 9, 6, 7, 4, 4, 2, 6, 5, 7, 4, 7, 4, 2, 3, 5, 5, 3, 4, 9,
1, 9, 4, 9, 3, 4, 9, 6, 9, 8, 3, 5, 2, 0, 3, 1, 2, 7, 7, 4, 5,
0, 6, 3, 2, 6, 2, 3, 9, 5, 7, 8, 3, 1, 8, 0, 1, 6, 9, 8, 4, 8,
0, 1, 8, 6, 9, 4, 7, 8, 8, 5, 1, 8, 4, 3, 8, 5, 8, 6, 1, 5, 6,
0, 7, 8, 9, 1, 1, 2, 9, 4, 9, 4, 9, 5, 4, 5, 9, 5, 0, 1, 7, 3,
7, 9, 5, 8, 3, 3, 1, 9, 5, 2, 8, 5, 3, 2, 0, 8, 8, 0, 5, 5, 1,
1, 1, 2, 5, 4, 0, 6, 9, 8, 7, 4, 7, 1, 5, 8, 5, 2, 3, 8, 6, 3,
0, 5, 0, 7, 1, 5, 6, 9, 3, 2, 9, 0, 9, 6, 3, 2, 9, 5, 2, 2, 7,
4, 4, 3, 0, 4, 3, 5, 5, 7, 6, 6, 8, 9, 6, 6, 4, 8, 9, 5, 0, 4,
4, 5, 2, 4, 4, 5, 2, 3, 1, 6, 1, 7, 3, 1, 8, 5, 6, 4, 0, 3, 0,
9, 8, 7, 1, 1, 1, 2, 1, 7, 2, 2, 3, 8, 3, 1, 1, 3, 6, 2, 2, 2,
9, 8, 9, 3, 4, 2, 3, 3, 8, 0, 3, 0, 8, 1, 3, 5, 3, 3, 6, 2, 7,
6, 6, 1, 4, 2, 8, 2, 8, 0, 6, 4, 4, 4, 4, 8, 6, 6, 4, 5, 2, 3,
8, 7, 4, 9, 3, 0, 3, 5, 8, 9, 0, 7, 2, 9, 6, 2, 9, 0, 4, 9, 1,
5, 6, 0, 4, 4, 0, 7, 7, 2, 3, 9, 0, 7, 1, 3, 8, 1, 0, 5, 1, 5,
8, 5, 9, 3, 0, 7, 9, 6, 0, 8, 6, 6, 7, 0, 1, 7, 2, 4, 2, 7, 1,
2, 1, 8, 8, 3, 9, 9, 8, 7, 9, 7, 9, 0, 8, 7, 9, 2, 2, 7, 4, 9,
2, 1, 9, 0, 1, 6, 9, 9, 7, 2, 0, 8, 8, 8, 0, 9, 3, 7, 7, 6, 6,
5, 7, 2, 7, 3, 3, 3, 0, 0, 1, 0, 5, 3, 3, 6, 7, 8, 8, 1, 2, 2,
0, 2, 3, 5, 4, 2, 1, 8, 0, 9, 7, 5, 1, 2, 5, 4, 5, 4, 0, 5, 9,
4, 7, 5, 2, 2, 4, 3, 5, 2, 5, 8, 4, 9, 0, 7, 7, 1, 1, 6, 7, 0,
5, 5, 6, 0, 1, 3, 6, 0, 4, 8, 3, 9, 5, 8, 6, 4, 4, 6, 7, 0, 6,
3, 2, 4, 4, 1, 5, 7, 2, 2, 1, 5, 5, 3, 9, 7, 5, 3, 6, 9, 7, 8,
1, 7, 9, 7, 7, 8, 4, 6, 1, 7, 4, 0, 6, 4, 9, 5, 5, 1, 4, 9, 2,
9, 0, 8, 6, 2, 5, 6, 9, 3, 2, 1, 9, 7, 8, 4, 6, 8, 6, 2, 2, 4,
8, 2, 8, 3, 9, 7, 2, 2, 4, 1, 3, 7, 5, 6, 5, 7, 0, 5, 6, 0, 5,
7, 4, 9, 0, 2, 6, 1, 4, 0, 7, 9, 7, 2, 9, 6, 8, 6, 5, 2, 4, 1,
4, 5, 3, 5, 1, 0, 0, 4, 7, 4, 8, 2, 1, 6, 6, 3, 7, 0, 4, 8, 4,
4, 0, 3, 1, 3, 9, 8, 9, 0, 0, 0, 8, 8, 9, 5, 2, 4, 3, 4, 5, 0,
6, 5, 8, 5, 4, 1, 2, 2, 7, 5, 8, 8, 6, 6, 6, 8, 8, 1, 1, 6, 4,
2, 7, 1, 7, 1, 4, 7, 9, 9, 2, 4, 4, 4, 2, 9, 2, 8, 2, 3, 0, 8,
6, 3, 4, 6, 5, 6, 7, 4, 8, 1, 3, 9, 1, 9, 1, 2, 3, 1, 6, 2, 8,
2, 4, 5, 8, 6, 1, 7, 8, 6, 6, 4, 5, 8, 3, 5, 9, 1, 2, 4, 5, 6,
6, 5, 2, 9, 4, 7, 6, 5, 4, 5, 6, 8, 2, 8, 4, 8, 9, 1, 2, 8, 8,
3, 1, 4, 2, 6, 0, 7, 6, 9, 0, 0, 4, 2, 2, 4, 2, 1, 9, 0, 2, 2,
6, 7, 1, 0, 5, 5, 6, 2, 6, 3, 2, 1, 1, 1, 1, 1, 0, 9, 3, 7, 0,
5, 4, 4, 2, 1, 7, 5, 0, 6, 9, 4, 1, 6, 5, 8, 9, 6, 0, 4, 0, 8,
0, 7, 1, 9, 8, 4, 0, 3, 8, 5, 0, 9, 6, 2, 4, 5, 5, 4, 4, 4, 3,
6, 2, 9, 8, 1, 2, 3, 0, 9, 8, 7, 8, 7, 9, 9, 2, 7, 2, 4, 4, 2,
8, 4, 9, 0, 9, 1, 8, 8, 8, 4, 5, 8, 0, 1, 5, 6, 1, 6, 6, 0, 9,
7, 9, 1, 9, 1, 3, 3, 8, 7, 5, 4, 9, 9, 2, 0, 0, 5, 2, 4, 0, 6,
3, 6, 8, 9, 9, 1, 2, 5, 6, 0, 7, 1, 7, 6, 0, 6, 0, 5, 8, 8, 6,
1, 1, 6, 4, 6, 7, 1, 0, 9, 4, 0, 5, 0, 7, 7, 5, 4, 1, 0, 0, 2,
2, 5, 6, 9, 8, 3, 1, 5, 5, 2, 0, 0, 0, 5, 5, 9, 3, 5, 7, 2, 9,
7, 2, 5, 7, 1, 6, 3, 6, 2, 6, 9, 5, 6, 1, 8, 8, 2, 6, 7, 0, 4,
2, 8, 2, 5, 2, 4, 8, 3, 6, 0, 0, 8, 2, 3, 2, 5, 7, 5, 3, 0, 4,
2, 0, 7, 5, 2, 9, 6, 3, 4, 5, 0, };
uint8_t *arr = (uint8_t*) &buffer;
int ***(uint8_t *arr, int x) {
}
It's done this way.
2022-05-12 4:45 AM
Note that it's conventional to use ALL UPPERCASE for #defined names - to distinguish them from variables (or functions).
uint8_t *arr = (uint8_t*) &buffer;Your pointer arr is redundant here - why not just use buffer direct?
If your issue is now resolved, please mark the solution:
2022-05-12 6:17 AM
then you cannot use buffers that are not 1000 long in that foo() function.