2022-12-12 03:50 AM
After installing a new compiler (9-2020-q2-update) with the Toolchain Manager I get the following Error.
No editor descriptor for id org.eclipse.cdt.ui.editor.CEditor
I am using STM32CubeIDE 1.11.0.
I have tried to change the workspace or a fresh installtion of the IDE but nothing works.
After a fresh installion everything works fine until I install another compiler.
Thank you for your efforts
Solved! Go to Solution.
2022-12-14 02:55 AM
In a way, yes.
If you already have the toolchain from a previous version of CubeIDE you can click the "Add Local..." button in the Toolchain manager to point to it.
If you don't already have it you can download version 1.7.0 from the st.com website and point to the toolchain folder (also using Add Local...):
C:\ST\STM32CubeIDE_1.7.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools
You don't need to launch 1.7.0 or anything, you can download it just to point to its local toolchain installation.
2022-12-13 01:08 AM
Hello there!
I'm fairly certain that you are facing the new issue that my colleague Mattias is mentioning in this thread:
https://community.st.com/s/question/0D53W00001zeSZcSAM/stm32cubeide-intool-update-issue
It might work if you remove CDT from the available software sites:
We are currently investigating this issue further!
2022-12-14 01:03 AM
Hi,
Thank you for your reply.
I have tested your suggestion but at the moment I always get the error shown below.
I have already tried this on a connection without proxy and anti-virus but the result is still the same.
If I understand it right, the updates have been stopped for the moment. My assumption is that it is related to this.
2022-12-14 01:38 AM
Yes, for now we have stopped most ways to update in order to stop users from accidentally breaking their installations. I'll be sure to update here if we find another safer way to do updates. Sorry for the trouble!
2022-12-14 01:43 AM
Is it possible to install the GNU Tools for STM32 manually? Unfortunately I could not find any information or installation files about this.
2022-12-14 02:55 AM
In a way, yes.
If you already have the toolchain from a previous version of CubeIDE you can click the "Add Local..." button in the Toolchain manager to point to it.
If you don't already have it you can download version 1.7.0 from the st.com website and point to the toolchain folder (also using Add Local...):
C:\ST\STM32CubeIDE_1.7.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools
You don't need to launch 1.7.0 or anything, you can download it just to point to its local toolchain installation.
2023-01-06 03:39 AM
Hello,
I've got the same issue after downloading Darkest Dark theme from Eclipse Marketplace, suddenly the IDE cannot open my code. I want to try this option as I have 1.11 and 1.7 installed, but I do not have Toolchain Manager appear in Preferences/STM32Cube? Only Device Config, Firmware Updater and MPU Serial
Thanks!
2023-02-09 08:26 AM
Same issue.