cancel
Showing results for 
Search instead for 
Did you mean: 

Error in final launch sequence - No device on target

alw
Senior

I have a NUCLEO-G491RE board connected to a PC running STM32CubeIDE v1.17.0. On first connection I was prompted to update the firmware on the board, which I did. On successful completion of the update I disconnected and reconnected the board, but the download failed with the attached message. 

I have tried several USB cables and also with and without an intermediate USB hub to eliminate these possibilities.

What is the solution please?

11 REPLIES 11

Hello @alw ,

Further to the picture provided on message. I recommend that you change the jumper on CN11 to JP6.

IMG_2178.jpeg

Thanks.

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

alw
Senior

Problem solved, it was just jumper link settings.

JP5 (5V_SEL): 5V_STLK

JP6 (IDD):        On

JP7 (BOOT0):  Off

Suggestion, rather than the error messages that are provided, have ones that advise users to check thatthese links are correctly fitted.