cancel
Showing results for 
Search instead for 
Did you mean: 

ctrl + z not working in the CubeIDE

MichalPorazko
Associate III

It suddenly stopped working 

2 REPLIES 2
STTwo-32
ST Employee

Hello @MichalPorazko 

I've just tested on the STM32CubeIDE V1.18.1 and it works fine (as expected).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

No I don't mean that its nor working in every version of the STM32CubeIDE V1.18.1, I m trying to figure it out if I maybe clicked something causing the ctrl + z to not work. 
Now its suddenly working but I was wondering if there is some kind of setting which can be accidently turned off and hence also disabling the crlt + z command